Elo Driver for Windows XP, Windows Vista and Windows 7

                     Release 5.1.1
                    March 05, 2010
                     Elo TouchSystems
         A Division of Tyco Electronics Corporation


Elo Driver contains native 32 and 64 bit drivers designed for 
Windows XP, Windows Vista and Windows 7, a setup program, video alignment 
program, control panel program, tool tray application and right 
button application for Elo TouchSystems' touchmonitors.  

=============================================================

Notes: 

  This Driver's User Manual is valid for all drivers version 4.X.X and 5.x.x

  
=============================================================
Supported Touchmonitors and Elo Touchscreen Controllers
=============================================================

   - All Elo Entuitive brand touchmonitors with a USB
     controller

   - Elo USB Controllers (IntelliTouch(R) 2216, 2600, 2500U,
     2700, 2701, AccuTouch(R) 3000U, CarrollTouch(R) 4000U, 
     4500U, Surface Capacitive 5000, 5020), APR 7010.

   - All Elo Entuitive brand touchmonitors with an internal
     serial controller

   - Elo Serial Controllers (IntelliTouch(R) 2500S, 2310B, 
     2216, 2310, 2300, 2700, 2701, AccuTouch(R) 2210, 
     CarrollTouch(R), 4000S, 4500S, Surface Capacitive 5000, 5020)


================================================================
Installing Elo Driver on Windows XP, Windows Vista, Windows 7
================================================================

Note: you must have administrator access rights on your 
Windows XP or Windows Vista to install Elo Driver for Windows. 

Shutdown your computer and connect your touchmonitor as described
in the accompanying documentation. Restart your computer.


Browse to the directory containing the driver installation 
package files. 

Double click on EloSetup.exe to run the install application.

=================================================================
Uninstalling Elo Driver on Windows XP or Windows Vista
=================================================================

1. After Windows loads, click the Start button, click Settings, 
   and then click Control Panel. 

2. Double-click the Add/Remove Programs icon or Programs and Features

3. Select Elo Driver from the list of uninstallable programs.

4. Click the Add/Remove or Uninstall button then follow the directions on
   your screen.

===========================================================================
To enable/disable the pre-calibration using registry:
=========================================================================== 
There is a flag "WriteNVRam" (data type is REG_DWORD) in the registry which
is used to enable/disable the pre-calibration. This entry is under registry
key "HKEY_CURRENT_USER\Software\Elo TouchSystems\".
 
The value of "WriteNVRam" is 1 for pre-calibration (write calibration data 
to NVRam); 

If the value "WriteNVRam" is 0, it means disabled pre-calibration (no longer
write calibration data to NVRam).
 
If the "WriteNVRam" entry does not exist, pre-calibration is the default action.
 
This entry is created during first time calibration after Elo installation.
 
This flag applies to 3-point calibration mode only.

============================================================================

==============
Contacting Elo
==============

www.elotouch.com

e-mail: eloinfo@elotouch.com

Elo TouchSystems
A Division of Tyco Electronics Corporation
301 Constitution Drive
Menlo Park, CA 94025
USA
Phone: (800) 557-1458
       (650) 361-4700
Fax:   (650) 361-4747

Elo TouchSystems GmbH & Co. KG
Haidgraben 6
D-85521 Ottobrunn
Germany
Phone: +49 (0) 89/60822-0
Fax:   +49 (0) 89/60822-150

Elo TouchSystems, NV
Diestsesteenweg 692
B-3010 Kessel-Lo
Belgium
Phone: +32 (16) 35-2100
Fax:   +32 (16) 35-2101

Copyright (c) 2010 Tyco Electronics
All rights reserved.